Dear Sirs
Does TI provide AFE solution like ZMDI ZSSC3138.
BRS
Nat
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Nat, yes, TI recently released the PGA900 which is a progammable resistive sensing conditioner with digital and analog outputs. The PGA900 has 2 AFE chains that include 24-bit sigma-delta ADCs. In addition, the PGA900 supports analog outputs (voltage ratiometric/ voltage absolute and 4-20 mA) as well as I2C, SPI, UART and OWI. Please refer to the PGA900 datasheet for more details, link below:
http://www.ti.com/lit/ds/symlink/pga900.pdf
Thanks,
JV
Nat, the PGA900 is a pressure sensor signal conditioner. At the moment, we don't offer the complete sensor (sense element + sensor signal conditioner). If you can provide me more details on what exactly you are looking for I could comment a bit more.
Thanks,
JV