In my application, I need to periodically measure the inductance of a coil that has voltages up to 12V across it. I would like to take measurements when there is no voltage across the inductor and it is in an isolated state. My circuit already accounts for this just fine.
My question is about the proper way to avoid damage to the LDC1612 when it is not actively taking measurements. Is the LDC1612 able to tolerate exposure of up to 12V if the device is set to shutdown mode? Or, alternatively, is it possible to protect the device by properly designing the impedance of the circuit such that the 12V comes from a high impedance path?