This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP007 package mechanical data

Other Parts Discussed in Thread: CC2650

I'm trying to debug a problem with the TMP007 sensor on a CC2650 SensorTag. The sample code provided for the SensorTag can't access the TMP007, which fails to acknowledge its I2C address. The same firmware appears to work fine for other people, so I'm wondering whether the TMP007 on my SensorTag could be damaged or incorrectly installed.

I've read the TMP007 datasheet and app note AN-1112 DSBGA Wafer Level Chip Scale Package (Rev. AG), which covers WLCSP packages in general. Unfortunately I haven't found the information I'm looking for.

Here's a photograph of the chip on my SensorTag:

First of all, is the circular dot at the lower left marking the location of pad A1 (on the underside)? Do the pads then continue A1, A2, A3 moving to the right and A1, B1, C1 moving up the image?

Second, is the package expected to be perfectly square with no corners missing? Here's another picture highlighting what appears to be damage to the upper two corners of the package:

I'm not sure whether the missing corner at the top right is deliberately cut off to indicate orientation, cosmetic damage during manufacturing or damage that could cause product failure.

  • Hi Robert,

     

    As your picture shows, A1 is in the bottom left corner as indicated by the pin A1 marking. The left side column is A, and are A1, A2 and A3  respectively, going up. The column on the right hand side is C; and the column in the middle is B.

     

    The missing silicon corners are not normal; it could very well be a manufacturing defect. From where did you get the evaluation kit? Perhaps you could ask for an exchange?

     

    Regards,

    Guang-Apps Sensing Products