This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Robust liquid level sensing with conductive fluids?

Other Parts Discussed in Thread: FDC1004, FDC2214

The FDC1004 allows use of the Out of Phase technique for robustness due to any hand interference. The example frequently given is a coffee maker. Suppose I now want to use salt water (conductive) in my coffee maker (yuck!). I think this suggests I should be using a part from the higher frequency FDC2x1x series, such as the FDC2214. Is there a similar technique as Out of Phase, but for the FDC2x1x series? It also looks like I'd lose the ability to shield electrodes, forcing use of an external driver.

Is FDC2x1x still the best choice for conductive fluids, despite these limitations?