This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Not getting accurate sensor readings (temperature as well as Humidity)

Other Parts Discussed in Thread: HDC1000

Hi,

I have designed sensor using HDC1000 as per guidelines given in application note and datasheet.

I have designed 2 boards one is CPU board and other is sensor board. senor board goes into CPU board with locking connector.

As per datasheet, sensor should be kept away from the CPU, display etc. So distance between CPU and sensor is approximately 1 inch.

Problem is temperature is 2 deg. higher side and humidity is 12% on lower side

My question is

"How much ideal distance between CPU, display and actual sensor should be kept to get accurate readings ?"