This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP112 Calibrate Calculations

Other Parts Discussed in Thread: TMP112

Hi,

For the formula that was written to the data sheet of the TMP112, please let questions.

1) Constant of Accuracy (25 ℃) in the data sheet (SBBOS473D) page23 equation (2) and formula (4) is "0.3 ℃".

     And I will think "+0.5℃" .← Is it correct in this understanding? (Reason: page5 Accuracy = it is written, ± 0.5 ℃)

2) Constants of page23 equation (11) Slop2 (MAX) is "4.5m ℃ / ℃".

     And we will think "5m ℃ / ℃". ←Is it correct in this understanding? (Reason: Table14 it is written, 5m ℃ / ℃)

Best regards