I’m looking for a temperature device where I can attach a resistor to set when a particular temperature has been read.
As an example, if I attach a 10K resistor it will output a low when 65C is met or I could attach a 8.2K and the device will output at 62C. In other words a full temperature module in a SOT123, with an output that triggers at a certain temperature set by an external resistor.
I don’t need super accuracy – say +-2.5C.
Do we have anything like this?