This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About the firmware update



 

Hi

  sorry, I miss-type the Firmware as "Firmwok".

  By the way, when I try to update the firmware with file nanmed "OPT9220A_0v31.tie" with 3D-Explorer version of V1.22, the 3D-Explorer Right Panel show "ERR-CdkBoardUndefined".

 

Thanks

 

Junbin

 

 ==================


Hi:

 

   we have bought your 3DTOF-CDK-SBA and I fine a file nanmed "OPT9220A_0v31.tie" and I update the firmwork with this file with 3D-Explorer version of V1.22. But I failed. Then I try to uninstall the 3D-Explorer version of V1.22 and install the "3D-Explorer-v1.9-SBAC122" and I try to  update the firmwork with this file "OPT9220A_0v31.tie"  and I failed again because it need the filename extension with "tip" not "tie". So I change the file name "OPT9220A_0v31.tie" to "OPT9220A_0v31.tip" to upgrade the firework. The result said "write complete" and the  3DTOF-CDK-SBA can't work anymore.......

  

   Please help me

Best!

 

Junbin