HI
Kindly clarify the following queries.
1) Regarding the Shield pin.
2)How to use the Shield pin, what material should I use for shield pin , where to stick it?
3)There is statement called as "Maximum Offset Capacitance: 100 pF", what does it mean?
4) What does this statement mean by "Maximum Shield Load: 400 pF"?
5) How stable will the O/P be??
6)will it be effected by humiditity and other EM radatitions?