I am testing the TDC1000 with the LNA in resistive coupling mode and using just the receiver i.e. not using a single transducer with the transmitter also connected the transducer. I have removed R42 from my evaluation board and replaced C43 with a 900 resistor.
Since the LNA non-inverting input is biased to VCOM sometime after trigger, I see the following:
Where probe 1 is the trigger, probe 3 is the output from BUFF_PGA, and probe 4 is on the transducer.
My question is it required to capacitor couple the transducer and bias the input to Vdd/2 to get this to work properly?
I have my TDC1000 eval board set up as shown below: