This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USE TDC1000-TDC7200 EVM to develop a gas flowmeter



I want to use tdc1000-tdc7200 evm to develop a gas f;owmeter. can you provide  some reference documentation or design notes for me. thank you

  • The TDC1000-TDC7200 EVM is targeted at liquid level, concentration and flow applications utilizing 1Mhz transducers. For gas or air applications utilizing 200kHz or less we recommend the TDC1000-GASEVM as it provides the high voltage excitation required for gas applications.

    Best regards,