I have found something interesting....
The TDC1000 transmits pulses ie: square wave.
When I connect up a piezo disc (the 1 MHz one supplier with the eval board) and attach the disc to metal conduit I get very strange results.
The recieving sensor picks up the tx signal (with almost no delay) along with the signal as attenuated and delayed by the liquid betwen the sensors.
It seems that there is more than one signal path.
Now a square wave is a fundemental and infinite odd harmonics and I think that these higher frequencies are causing problems.
I tried the exact same sensors with a signal generator and with a square wave I get identical results but with a pure sine wave I only get a signal with the correct delay time on a sensor in line with the tx.
So question, why does the TDC1000 ouptut a square wave when I believe (for much better results) it should be a sine wave?