Hi TI!
Please tell me how to connect [B17] PIN OPT8241
[B17] PIN OPT8241 - VSUB_BIAS how to connect?
from documents it is not clear what it is.
From the scheme SDK is not clear how the circuit with transistors and what it is.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI!
Please tell me how to connect [B17] PIN OPT8241
[B17] PIN OPT8241 - VSUB_BIAS how to connect?
from documents it is not clear what it is.
From the scheme SDK is not clear how the circuit with transistors and what it is.
Thank you.
Hi Ruslan,
Thanks for your interest in the product.
VSUB_BIAS has to be connected to -5V (negative supply). The connections are given in the schematic files and they are as follows:
As per the schematic, U1 and U2 are the transistors to be connected. Can you help me understand what connections you are asking about?
Regards,
Subhash Chandra
VCC_5V0_MINUS_FSC -->VCC_5V0_MINUS-->VCC_OUT_5V0_NEG-->VOUT ???
If I use the power 3.3 volts for the circuit. What to apply for this port?
Under the scheme, I do not understand how the work transistor unit.
I passed on the circuit and came to Vot /
To be honest, I do not know right now how to connect this pin.
Hi Subhash
I now understand how it works.
I was left with two questions.
1) receives 5 volts in the circuit are mandatory condition on the pin [B17] must be submitted at -5 V "ILLUM_EN" at the moment when there is no exposure to [B17] + 3.3V supplied. I understand correctly?
2) I can directly [B17] to connect to -5, without the transistor unit. What will then be the consumption and the risk of a direct connection?
Ruslan,
There is no functional risk in keeping the -5V on all the time. But depending on the ripple on the -5V, there may be a small noise degradation due to the fact that the negative supply is on even during the readout and ADC sampling of the sensor data (The effect negligible in most cases because of the differential nature of the whole signal pipeline). If you plan to connect directly, we suggest that you minimize the ripple to ~50mV level.
Regards