TIDA-00508 accuracy of 4-point calibration is 0.9-degree over 0C to 85C. Does the 0.9-degree accuracy inclue the sensor cap temperature drift?
customer use LDC1314 in knob application, there are four coils. Is it suggested to having the four coil with same trace length?
Now we observe TIDA-00508 with 4-point calibration accuracy of about 0.9-degree. To improve the accuracy, what is the suggested average points based on reaching 75 rotation per minute?