Hi
We are about to evaluate FDC2214 for gasoline level sensing.
FDC2214 is good for EMI with its architecture but it doesn't have shield driver.
On the datasheet, FDC1004 is recommended when the presence of interferences such as human hands is assumed.
So, I have following questions.
1. Should we choice FDC1004 which has the shield driver if we want to avoid the presence of interferences?
2. We want to use FDC2214 because it has good spec.
Are there any way to avoid the interferences (human hands, etc) using FDC2214?
regards