I have a patented sensor that uses fringing fields to sense moisture on top of plastic sheet. Two runs interleaved on the top do the sensing at 13.56 MHz. From dry to totally wet involves 1 pf change. Must work from 29 F to 129 F. Would the FDC1004 work in this? I guess one connection (active) goes to one run; ground goes to the other run and shield goes to the bottom with fr4 in between. Fringing field is above flat sensor. I just need one sensor not 4. Its normal dry capacitance is 62 pf. Please point me in the right direction documentation wise. Thank you