Hi,
We wanted to use the capacitive senor for non contact movement analysis, The apparatus we have in mind is set up in such a way that the body moves only perpendicular to the sensor plate .We would love if you could help us oout with the follwing questions:-
- Can I use the sensor to measure disatance of the body as show in the TI vedio demostrations using an arduino to read I2C(distance < 3cm)?
- Can I get a sample data rate of at least 2K values per sec with FDC2214 +Arduino System?
- What are the typical materials that the moving body be made of for maximum sensitivy such that the sensor plate can pick up changes in capacitance easily?Can I increase sensitivity by Grounding the material(Conductor)?
- Will the device detect changes if I put the object around 3cm from the sensor plate and a change in +/- 1 cm?also, wats the max. distance that the sensor plate can pick up the changes in capacitance?
- Note that the moving body only moves perpendicular to the sensor plate.