hi,
In my application, I am using LDC1000 for measuring the inductance of a coil which is wounded on a nonmagnetic electrically conducting hollow cylinder with variable magnetic core.I experimented this with LDC1000EVM, unfortunately am not getting proper result. after some investigation I got to know that the sensor frequency is the trouble for my application. if the sensor frequency is more than 40KHz eddy current effect be predominant than the permeability effect. In LDCEVM GUI I seen one option sensor frequency which is having value from 2.5KHz to 500KHz, I don't know what exactly it means. please give me some suggestions in which I can use LDC1000 for my application or how can I change the value of Fsensor value in 2.5KHz or below 10Khz.?? is it possible to fix the sensor capacitor value to in micro Farad range??