This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC1050 excel calculator for dew point

Other Parts Discussed in Thread: HDC1050

Dear Sir

Our end customer would like to know the dew point of HDC1050

Does TI have dew point calculator or any design guide for dew point ??

Thanks

Dew Point: +/- 2.5 °C (-44 °C to 79 °C )

Calculated measurement of temperature at which moisture in the air will turn to water based on the humidity and temperature measurements