Hello,
We'd like to use FDC2212 for the people proximity detection. There are still some unclear items need to consult you. Thx.
Q1, just as the one of FDC1004, could we use the "active shielding" method onto FDC2212, in order to reduce the interference between two channels?
Adding GND to act as shielding is not so good, which would reduce the sensitivity of detection range.
Q2, for the single-end sensor solution, what if the antenna pad is connected to INxB instead of INxA? any difference between them?
Many thx.