Hello,
We performed some EMC immunity tests on our FDC2214 EVM, and got some interesting phenomena, which could not be understood by us. Could you give some comments? Thx.
Phenomena:
1, As shown in GUI, there are big variation of raw data, if the injected interference frequency is at the resonant frequency and its 3, 5, 7, 9, 11 times frequency. Our resonant frequency is around 5.47MHZ, then it's would more than 10MHZ at 3 times resonant frequency. Then, why could our sensor still detect it since the max active frequency is 10MHZ mentioned in the datasheet?
2, Also, the variation, on these frequency point, is not always toward one direction but positive change at certain frequency and negative change at other frequency. Why is ti?