Hi,
The datasheet for the TDC1000 indicates a measurement range of up to 8 ms. The datasheet also indicates that the min operating frequency is 0.06 MHz.
Using a 1.28 MHz clock (for example), the TDC1000 can be configured for echo listening periods of up to 15 ms. (Based on Figure 38: Standard TOF Measurement.)
What is the source of the 8 ms value for the measurement range?
I would like to achieve a longer listening period than 8 ms - preferably something closer to 30 ms. (ie with a 0.64 MHz clock).
On our prototype board with a 1.28 MHz clock, I am able to detect signals up to 8.5 ms or so. When the input signal is detected, the signal (pulse) going in to COMPIN looks fairly strong. After making a very minor change in the distance to slightly increase the TOF, the pulse is gone.
I would expect that the pulse would degrade slower and not suddenly around 8.5 ms.
In parallel to my own debug efforts on this, I thought that I would ask if there is something in the TDC1000 that the 8 ms time is based on that might be at play here.
Thanks,
Wayne
PS. My application is for distance measurement through air. I have a boost circuit on my transmit signal to increase the voltage to my 40 kHz emitter to improve the range. And I have looked at the PGA450 but it doesn't appear to meet my need to synchronize more than one of them together.