Hi there,
I am planing to implement a LDC1312 for a linear distance measurement device, I wanted to calculate the change when placing the sensor at two different distances(min sensible distance and max sensible distance) by theory before I move into implementation,so that I can have a RANGE of values which I can work with. Is there any simulation I can do in this regard?
I am planing to use a circular coil(thickness and turns not yet decided) and metal object will be a copper plate parallel to each other.