This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7200, where to connect the TRIGG pin, when discrete front end circuit is used instead of TDC1000 .

Other Parts Discussed in Thread: TDC7200, TDC1000

Dear Specialists,

My customer is considering TDC7200 and discrete front end circuits.
Not using TDC1000.

In this case, could you advise where to connect the TRIGG pin ?

He thinks TRIGG pin seems to control TDC1000, so it should be floating, pull up or no connection.

Could you please advise?

Also, I am happy you send an example design for discrete front end.

I appreciate your great help.

Best regards,

Shinichi