Hello!
We got the following task: we have the round plastic container, 33mm diameter and 70mm tall, with some (water based) liquid in it. The container is disposable, and firmly attached transducer is not possible. We need to feed a pipette tip until touching the liquid inside the container (1-3 mm accuracy is ok). We got 2 kind of transducers - SMD10T2R111 and 400PT160 for water and air application.
First I experimented with water application. I glued the 1mHz transduser on the bottom of container and coonected it to my TDC1000-C2000EVM, but with default settings id does not sense the water level at all, and eved does not react on presence or absence of water inside, and nothing seen on my oscilloscope, I got the echo signal on COMPIN, but it does not change the shape.
Then I attached the 400PT160 transducer, and run the EVM again. this time I just trying to see any reaction to moving the transducer near the solid surface, but nothing happend again.
What am I doing wrong?
Thank you!