Hey Optical sensing team,
I noticed in the datasheet, it mentions the following:
"The OPT3001 has an automatic full-scale range setting feature that eliminates the need to predict and set the optimal range for the device. In this mode, the OPT3001 automatically selects the optimal full-scale range for the given lighting condition. The OPT3001 has a high degree of result matching between the full-scale range settings. This matching eliminates the problem of varying results or the need for range-specific, user-calibrated gain factors when different full-scale ranges are chosen. For further details, see the Automatic Full-Scale Setting Mode section."
Am I correct in assuming that this means as long as the register settings are correct, you can just populate the part on the board during factory assembly without the need to do any sort of calibration process?
Thanks!
Brian Antheunisse