Other Parts Discussed in Thread: PGA900, PGA309, PGA300
Hello,
I am interested in measuring the output of a bridge pressure sensor, however the electronics must be able to withstand operating at 150 deg C. We are using a high temperature MSP430, and originally we were going to use a PGA309. However, I haven't been able to find any high temperature EEPROM. This makes me think I should use the PGA900, especially since its output could be read over I2C from the MSP430 microcontroller we are using without requiring a separate high temperature ADC as would be necessary with the PGA309.
However, the idea of writing firmware for the PGA900 sounds like it would take a lot of time. I would really just like to be able to control the PGA900 over I2C and read data without having to write any firmware for it. Is this possible?
Thanks,
Hunter