Hello,
Currently, the customer would like to use the copper wires which is sealed in the acrylic bar as sensor for water level sensor.
And the level sensor and GND sensor are adjacence.
The copper wire which is removed from the conductive wire.
The copper wires are 1mmφ and Acrylic wire is 3.5mmφ
Can we use that wire?
Could you please let me know the φ vs. sense length if we use copper wire as the sensor?
Could you please contact to the following e-mail address directly
I would like to discuss internally due to there are some customer confidential information.
asaka-r@clv.macnica.co.jp
Best Regards,
Ryuji Asaka