This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000 Measurement accuracy

Other Parts Discussed in Thread: TDC1000

Hello,

Now, we are considering the ultrasonic sensor to the gas flow meter.

I can't decide the detection method between CORRELATION TYPE and TRIGGER TYPE.

And so I have questions about TDC1000.

 <Specifications>

  Target Gas : CH4

  Placement  : 45°Angle

  Diameter (D): 20-600mm

Resonant frequency:200kHz(In-House transducer)
  
Flow speed : 20-30m/s

Q1.I think that output voltage swing of approximately 20V is necessary to improve measurement accuracy.

  Is it enough to measure in the output voltage swing of 5V?

Q2.Do you have a function to correct or improve the distortion of the received waveform by noise

  caused in TDC1000?

Best regards,
Seishin

  • In cross-correlation method the echo signal is digitized using an ADC and the delta-TOF between the downstream and upstream is found by "cross correlating" the upstream and downstream signals- often three point cross correlation is used.
    In zero-cross TOF measurement method ( TDC1000 approach) the echo signal is filtered and amplified to about 2 V and then using two comparators "STOP" pulses are generated to measure TOF for upstream and downstream referenced to a START pulse. Therefore, to achieve optimal accuracy the signal at the input of the comparators needs to maintain at approximately 2 V range. This should be done by a combination of driving the sensor with proper-level of energy and in the mean time filtering and amplifying the signal with right amount of gain, please refer to the application note snaa284 at the link below for more details:
    www.ti.com/.../snaa284.pdf