I have several LDC1000EVM's, none of them will stay connected to the Sensing Solutions EVM GUI V1.8.8 rev.A.
I need an answer ASAP, or the part will not be consider for a project.
Best regards,
Keith Pant
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have several LDC1000EVM's, none of them will stay connected to the Sensing Solutions EVM GUI V1.8.8 rev.A.
I need an answer ASAP, or the part will not be consider for a project.
Best regards,
Keith Pant
Hi Keith,
My apologies for the problems with the LDC1000EVMs you have experienced. What version of Windows are you using?
In addition, can you provide more information on your application? There may be an LDC device better suited than the LDC1000.
Regards,
ChrisO
Chris,
I am on window 7 64 bit system.
The GUI works fine with TI's FDC2214EVM.
Sorry, I cannot discuss this application on any Forum do to company restrictions.
Right now I just need to evaluated inductive sensing technology and the LDC1000EVM will allow me to do this, if a can get to work with the GUI.
Later on, I can consider better options for this application.
Best regards,
Keith Pant
Chris,
I had already ruled out a bad EVM, due to trying several of the units and getting the same results. The EVM is active on the USB port, verified by going to control panel, then system.
I down loaded the snac058 and installed it. It indicated the firmware was out of date. The firmware was updated and now LDC1000EVM works with both GUI's.
Thank you for the help.
Best regards,
Keith Pant