Hello, i am working with ultrasonic water flow sensor and developing my own PCB to interface the sensor with TDC1000. I have a misunderstanding in TDC1000 active channel definition; to measure the water flow rate i should use mode 2 for measurement, which define channel 1 as TX1/RX1 and channel 2 as TX2/RX2. Does TDC1000 have the ability to internally change the channel definition for the different measuring mode or should i connect it myself by the hardware ?What is the right channel connection to measure in mode 2 ?
Thank you