Hi Bharath,
Can i directly connect SUB_BIAS pin to 0 V on all the time. if i do this,is there have any risk about this?
what is your advice about this?
Regards
None
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Bharath,
Can i directly connect SUB_BIAS pin to 0 V on all the time. if i do this,is there have any risk about this?
what is your advice about this?
Regards
None
It is ok to connect SUB_BIAS pin to 0V at all time. All of the system estimator tool's simulations are infact done with SUB_BIAS = 0V. Negative SUB_BIAS voltage is used in the OPT8241-CDK to improve the demodulation contrast.
Regards
Hi,
It is ok to connect SUB_BIAS to 0V all the time. Improvement due to use of negative bias depends a lot on operating conditions (Probably about 10-30% better depth resolution depending on Modulation frequency, VMIXH voltage. Improvement is more noticeable at modulation frequencies greater than 40MHz). It is best to use an option for negative voltage SUB_BIAS during prototyping. Once the operating conditions are fixed, you can do two expts -
- Turn on SUB_BIAS, take a note of the performance (standard deviation of phase at a fixed distance)
- Turn off SUB_BIAS, record performance again.
Compare the two performances and decide on whether you need SUB_BIAS. If you don't need it, you can DNP (Do not populate) the parts when you do the production version.
Regards