Hi TI,
I have question about LM3429,please see the follow, I hope you can help me solve it.
Q1: the Pin number 7 nDIM: as describle in Pin function,it seems like when the voltage of the pin less than 1.24V,so LM3429 will not function,it is all right?
Q2: In LM3429 Datasheet page 13 The formula(as describle in the follow picture). we can adjust Rcsh to change the LED current, my question is if the Rcsh is setting OK,so the current of led is ILED,but when I use PWM dimming the light, the PWM Duty ratio assumed D, so the current of LED(Io)whether equal to Io=D*ILED.
about Q1&Q2,I want to know what my understand is right or wrong?
Thanks&Regards
None