Hi guys,
There's only one sentence about the low power mode of OPT9221. I can't infer the power consumption from what is given in datasheets. Can anyone help me out? Any data or experiment data? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi guys,
There's only one sentence about the low power mode of OPT9221. I can't infer the power consumption from what is given in datasheets. Can anyone help me out? Any data or experiment data? Thanks.
I did some experiments myself. Here is what I got.
Scenario 1: Depth Camera is streaming with 55% illumination, 8% integration time and 60 fps. The power consumption of the entire evaluation board is around 2W.
Scenario 2: System is idle which means depth camera is not streaming.(Basically, I only turn on the power). The power consumption for the idle system is around 1W.
Scenario 3: System is standby which can be approached by changing the registers. The power consumption when the board is standby is around 0.5W.
Does scenario 3 suggest that OPT9221 low power mode still consumes 0.5W? This is quite a huge standby power for just a MPU, or this is not only OPT9221, something else is still working when OPT9221 is standby?
Please, any TI guys can answer my questions? This is very important.
Justin,
Sorry for the late reply. You can use the CDK schematics to infer the power supply recommendations. Each DCDC/LDO rail has a listed maximum current. What is the standby power you are aiming for?
If standby power is a serious concern, we can take the discussion to a private mail thread. Please send us an email at ti-3dtof@list.ti.com for a detailed discussion on power.
Regards