This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP007 for temperature measurement

Other Parts Discussed in Thread: TMP006

Hi,

I'm considering to design a temperature measurement system by TMP006/007. and the requirements are below:

1. Detect distance: 30cm ~5m

2. accuracy: +/- 1'C

Distance is far and FOV should be very small. I'd like to know if an optical system (lens system) is needed to archive these requirement?

Is there any design guide for the detecting distance and accuracy?