The image above is taken from SLDS209A pg118.
1. Which register controls S2?
2. When S2 is closed, don't the two 40k resistors act as a voltage divider? Would that limit the voltage at the positive terminal of the op-amp to .625 VDC?
3. Should DACCAP be left disconnected, or should it be connected to the negative terminal of the controller via a 100nF cap, as in the PGA900EVM and PGA900 4-20 Mode TINA Spice Model?