This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP007 Questions about range of measurement

Guru 16770 points

Hi

We have questions about accuracy of internal amplifier and measurement range.

1. When using TMP007,  what is the parameter attributed to measurement error?

2. We want to measure the target temperature up to 350 degrees.
     Would it be possible?

Best regards

  • There are many system and device variables that contribute to measurement error. Before we can discuss measurement error, the physical aspects of the system such as Field-of-View, size of object, distance, emissivity, other heat sources and convection air flow must be well defined. After these effects are understood and calibrated, the sources of measurement error are primarily due to large local temperature transients and device to device variation.

    Ren