I'm using a TMP007 in an application to measure air temperature of a tire. The sensor is in a aluminum tub, that on one end is a sealed connector for the I2C signals, the other end has a air chuck so that it's connected to a tire, the tube is 'sealed'. The air chuck threaded part ends up .5" from the face of the TPM007 (no window currently in front of the sensor) inside the tube. When I connect air to the air chuck, the temperature reads correct for maybe .5 seconds than displays a temperature way to hi.
The aluminum tube is black anodized on the inside. What would cause this? No window in front of the sensor? Sample rate to fast (every second)?
Please help
Thanks much.
Dan Ross