I have an FDC1004EVM device that works perfectly on my Windows 7 Professional laptop, but when I install the exact same applications on a Windows 10 laptop the application shows 'Not connected'.
If I look in device manager I can see the device gets recognized when I plug it in and is assigned to COM5. I have tried un-installing rebooting and re-installing the code. I have deliberately remove the device in device manager and let it re-install the "best" driver, but it still will not connect. I have tried running the application "As Administrator" and it still won't connect.
I am using v1.8.8 of the Sensing Solutions GUI.
Any suggestions?