This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91300 Labview vi for SWIF

Other Parts Discussed in Thread: LMP91300

Hello TI team,
I need to communicate / program the device  LMP91300 with LabWiev.
I read in the forum that you have VIs that you can use to implement the code.
How can I have the VI ?.
Thank you

  • Hi Vincenzo,
    I will try to find the Labview VI and will get back to you tomorrow. Can you please link the thread which you referred to in your question?

  • You're welcome. I hope it will help you with your design.
  • Hi Ben,

    my name is Stefano Anceschi, and I'm a Giudicissi's collegue.

    I'm trying to use labview routines you passed us, but I've some kind of difficulties, may you help me?

    The Demo Labview program cannot detect any board ( error - 1)

    I attached the log file generated by labview.

    What I'm doing wrong?

    Thanks

    16/06/20:13:16:24.0504:SCRIPT_EP:__log.txt not found:  Logs not enabled
    16/06/20:13:16:24.0504:SCRIPT_EP:CINT init params:cint -IC:\hardware\scripts\include -IC:\hardware\scripts -qlevel1 -Z0 
    16/06/20:13:16:24.0505:SCRIPT_EP:!!! 0 object(s) deleted by Reference Count Control !!!
    16/06/20:13:16:24.0517:SCRIPT_EP:Error: cannot open file "script_api.h"  (0)
    16/06/20:13:16:24.0517:SCRIPT_EP:Error: cannot open file "gen_access.h"  (0)
    16/06/20:13:16:24.0518:SCRIPT_EP:Error: cannot open file "gen_access.cpp"  (0)
    16/06/20:13:16:24.0518:SCRIPT_EP:Error: cannot open file "utils.h"  (0)
    16/06/20:13:16:24.0518:SCRIPT_EP:Error: cannot open file "utils.cpp"  (0)
    16/06/20:13:16:24.0519:SCRIPT_EP:Error: cannot open file "spi_auto_mode.h"  (0)
    16/06/20:13:16:24.0519:SCRIPT_EP:Error: cannot open file "spi_auto_mode.cpp"  (0)
    16/06/20:13:16:24.0519:BOARD_STATE:USB config: WINUSB_SUPPORT
    16/06/20:13:16:24.0519:UTILS:Simulator settings not found.  Continuing.
    16/06/20:13:16:24.0519:UTILS:Looking for image map file:C:\hardware\scripts\image_map.xml
    16/06/20:13:16:24.0519:UTILS:Image map file not found:C:\hardware\scripts\image_map.xml
    16/06/20:13:16:24.0520:CMD:return:DLL_COMMAND_RET_OK
    16/06/20:13:16:24.0520:CMD_API:Ack received.  Releasing API.
    16/06/20:13:16:24.0520:CMD_API:==== Command complete     ====
    
    16/06/20:13:16:24.0520:CMD_API:==== Starting new command ====
    16/06/20:13:16:24.0520:CMD_API:Waiting for API
    16/06/20:13:16:24.0520:CMD_API:Posting command
    16/06/20:13:16:24.0526:CMD:Processing ...
    16/06/20:13:16:24.0526:CMD:DLL_Board_Enum
    16/06/20:13:16:24.0526:BOARD_STATE:Skipping error board
    16/06/20:13:16:24.0526:BOARD_STATE:Board count:0
    16/06/20:13:16:24.0526:GEN:Dll version:2.0.0.5
    16/06/20:13:16:24.0526:CMD:return:DLL_COMMAND_RET_OK
    16/06/20:13:16:24.0526:CMD_API:Ack received.  Releasing API.
    16/06/20:13:16:24.0526:CMD_API:==== Command complete     ====
    
    16/06/20:13:16:29.0753:CMD_API:==== Starting new command ====
    16/06/20:13:16:29.0753:CMD_API:Waiting for API
    16/06/20:13:16:29.0753:CMD_API:Posting command
    16/06/20:13:16:29.0759:CMD:Processing ...
    16/06/20:13:16:29.0759:CMD:Dll_Board_Close:0
    16/06/20:13:16:29.0759:BOARD_STATE:board_close():0
    16/06/20:13:16:29.0759:BOARD_STATE:Board was not allocated
    16/06/20:13:16:29.0759:CMD:return:DLL_COMMAND_RET_OK
    16/06/20:13:16:29.0759:CMD_API:Ack received.  Releasing API.
    16/06/20:13:16:29.0759:CMD_API:==== Command complete     ====
    
    

  • Hi Stefano,

    Your SWIFEVM board may not have the correct firmware to use the Labview vi. If the board was shipped to you from us and worked with the TI Webench GUI it will not work with the Labview software. It will need to be updated.

    I will contact you to get you the correct firmware.

    Mike