Hi All,
I just joined the rotation program as an analog FAE and I would like to have an opinion from you about a request I received by a customer for the inductive sensing of an LDC1614.
The application is an encoder for motors. The customer wants to detect the rotation of a metallic disc.
The customer is facing some problems regarding the sensitivity of the LDC 1614 to capacitive influences, like moving a hand over the coils, which results in relatively large changes of the measurement result (about 0,5% of the measurement range).
Do you have some suggestions about how to compensate those influences, e.g. using differential coils? Or changing the coil shape or number of turns? Or adopting a particular method to improve the SRF?
The customer is going to use very small coils (2mm outer diameter) so with a very small inductance (approx. 0,41 µH according to WEBENCH tool), What about the resulting measurement range?
Using the LDC1614 EVM with the coils from 1-Degree-Reference-Design, the resulting range of the measurement result is 15,018,850 (decimal) which is why the noise has so small influence (percentaged).
Do you have some suggestions about how to estimate the resulting measurement range?
Many thanks in advance,
Regards,
Antonio Faggio