This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640 Timer resolution

Other Parts Discussed in Thread: CC2640, TDC1011

Hi, 

I'm planning to use CC2640 with TDC1011. In one of the application note, TMS320F28035-Q is suggested to be used with TDC1011 as it has 300ps accuracy. In my application, I need the level sensing accuracy of up to 10mm. But I'm still not sure about the resolution of CC2640 timers as there is no information given in the datahseet. Can anyone please let me know if I can use CC2640 without any accuracy issue?

Thanks in advance.