This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Request to provide the data which is transfer through Micro controller to TI GUI for FDC2214EVM

Other Parts Discussed in Thread: FDC2212, FDC2214EVM

Hello, 

We are working on one POC where we need to measure the oil level.

the POT dimension is  10x10x10 cm; oil : type 2 oil

At the POC point of view we are going to use the FDC2212 module and will interface it with our interfacing board.

So from the Firmware prospective we need to understand that what data use to transfer between T.I GUI and the FDC2214EVM?

Please provide your support to understand this so that we can define our firmware.

Regards, 

Sudhanshu