This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP007 EVM GUI - unable to change Total Conversion Time setting

I have a TMP007 EVM and the corresponding GUI. I am setting the power on, then setting device configuration up to be:


Conversion mode = Convert Local & Obj.

Total Conversion Time = 4 Sec (Idle for 3.5).

Transient Correction = Enable.


Then clearing both graphs on the "Temperature Limit Controls" tab, setting them to autoscale both X & Y and then starting Continuous Read.

The problem I have is both graphs start updating at a rate far quicker than once every 4 seconds and exporting to excel creates a lot more data than I want. It is as if the setting for Total Conversion Time is not being sent from the GUI to the sensor.

I've read the guide for the GUI and I can't see where I'm going wrong. Can anyone help? Thanks.