I have an application where I need to switch in the presence of a ~8mm diam x 8 L stainless cylinder at the largest range possible.
I know that larger coil diameters tend toward greater sensing range, but I have been unable to find any discussion of optimizing design for small targets. Is it better to continue the spiral all the way to the middle (choosing line and space to achieve the right inductance) or make a few tightly spaced turns at the largest diameter possible? It seems like, all else being equal, a single layer coil would be better than a 2 layer or 4 layer coil, because the target it as close as possible to the majority of the turns.
I've experimented with using a fixed, off-the-shelf reference coil which has seemed to help compared to a stacked coil configuration. What effect does LC resonant frequency have on sensitivity to small targets? The Excel tools for the LDC0851 do not take target diameter into account at all.
Thanks very much for any guidance you can offer.
Jesse