Hi,
I used a small diameter sensor (4mm) with lmp91300and I have some emc problems:
- esd immunity test (iec 61000-4-2): the device with 4kV is broken. I changed the Cby capacitor but I didn't see any improvements.
- Burst immunity test (iec 6100-4-4): the state of the output change for about 1ms. I fixed it adding a capacitor between the output and ground, but it reduce the switching frequency of the sensor.
- Conducted disturbances (iec 61000-4-6) . I can't fix the problem
Ps In the layout of NPN version I didn't place the D4 zener diode (between the supply and the output)