Dear all,
I do have two questions about these Hall sensors:
1) Is the DRV5023 aible to sense a current floating in a cupper pcb-trace below of it?
The current is a DCC signal (kind of PWM), an example can be seen at <http://www.modeltrainbuilder.com/DCC-operation.html>
What I want is detection of the current, which can be in the range of 20mA (lost carriage) till 2A (heavy loaded train).
The detection signal should be galvanic seperated from this DCC-signal, thats why I gues this DRV5023 can do the job???
2) Is the DRV aible to detect a small magnet?
The DRV will be build in the road, where the moving car will be controlled by a small magnet on the steering-axle. The magnet is 'following' the magnet-band. This band will be removed for a small part where the sensor is positioned. Looks like <forum.miniatur-wunderland.de/.../2377_Sensor_9366_1.jpg>. For the small magnet at the steering-axle an example can be <www.miniatuura.nl/.../Magneetband-fig11.jpg>
I hope it is clear what I mean. If not, just ask.
regards,
Willie