Hello,
If we connect the A0/ADD0 pin of TMP108/112 to the SCL pin, are there any problem ?
For example, is the following power sequence no problem?
1. Power ON the I2C pull up supply
2. Then Power On the temp sensor power supply.
Since the TMP108 A0 pin absolute maximum rating is (V+)+0.3V, the "V+" is powered on before I2C pull up power.
Are there other problem in this case?
Best Regards,
Ryuji Asaka