This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000 TDC7200 EVM GUI settings

Other Parts Discussed in Thread: TDC1000, TDC7200

1) For the "TOF_MEAS_MODE", I was wondering where I could find a description of what Mode 0, Mode1, and Mode2 are. Looked in the user guide and didn't see it.

2) What is the difference between the TDC_SELECT options on the graphing page of the GUI (I.e., Start-Stop 1, VS Start-Stop 5 or Start-Stop 345). If there's a more detailed guide to the GUI that has this information please let me know and I will read that before posting questions.

3) How long can I make the wire leads to the transducer before I run into trouble with capacitance, etc? (Steminc 1MHz)

4) To change the detection threshold in the GUI, it's the "ECHO_QUAL-THLD" setting? The smaller the voltage the lower the threshold I assume.

Thanks in advance!