This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ultrasonic transducers for flow to be used with for LNG

Other Parts Discussed in Thread: TDC1000, PGA450-Q1

Hi,

While I have the TDC1000 and the evaluation board and the stemic transducers suggested on the datasheet I also need the time of flight for the flow so I am looking for a prefabricated piece of pipework with the correct 1-1.5Mhz ultrasonic transducers already in place.  The demand for the gas is about 15g/s and the pipe is 12mm diameter.  Does anyone know where I can purchase these off the shelf?